Part Number: AM4372
Other Parts Discussed in Thread: TS5A3157,
Hi all,
I'd like to know about AM437x's boot mode.
My customer has selected the following boot mode.
Then, the application program is stored in the FLASH connected to the QSPI.
When power is input to the board in this state, it starts normally with QSPI boot.
However, when USB0 is connected in this state, QSPI boot will not be done.
Is this correct as the behavior of the device?
When the device is in this mode, it will boot with QSPI --> USB1 --> MMC0 --> USB0,
I think that QSPI boot will be done even if my customer connected USB0.
Best regards,
Sasaki