Part Number: AM4376
Hi,expert
In AM4376 datasheet DC Electrical Characteristics chapter, "All other LVCMOS pins (VDDSHVx = 1.8 V; x=1-11) "session, it mentions that when Ioh = 6 mA, min of Voh = VDDSHVx - 0.45, what is the exact meaning Ioh, max current? If it is max current, when use it as <6mA, for example, 4mA, dose it mean min of Voh should also decrease as V/R = I
The external connected LED, current input range is 4 mA~6mA, how to handle this case?