This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2HV: NOR Initialization Failed

Part Number: TDA2HV

Tool/software: Linux

Hi All,

I am working on TDA2HV custom board.

Our NOR is same as TDA2xEVM board but the only difference is in EVM board there is 64 MB NOR while our custom board has 32 MB NOR.

I want to run an example of csl_nor_read_write from Vision SDK 3.1 on custom board

So what changes I have to do in the example?

Hardware setup in both EVM and custom board are same.

I am getting NOR initialization failed ERROR.

Regards,

Pratik.