Part Number: AM5728
Tool/software: Linux
Hello,
I want to ask some questions about the dual-camera-demo.When I use the command:
dual_camera 2 -platform linuxfb
it showed the information:
CRTCs size: 800x480
Capture 0: Opened Channel
Capture 0: Capable of streaming
Capture 0: Init done successfully
ERROR:v4l2_queue_buffer:425: VIDIOC_QBUF failed: Bad address (-1)
ERROR:v4l2_queue_buffer:425: VIDIOC_QBUF failed: Bad address (-1)
ERROR:v4l2_queue_buffer:425: VIDIOC_QBUF failed: Bad address (-1)
Capture 1: Opened Channel
Capture 1: Capable of streaming
VIDIOC_G_PARM: Inappropriate ioctl for device
Only one camera detected
Running the demo on am57xx processor
w=800, h=600
and the whole LCD screen of the AM5728 was green.
I used the sdk4.0 and the camera was on the board (not the usb camera).
So could u give me some advice to solve the problem?
Thanks®ards!