This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMS320DM8168: how can set static IP in bootargs for ubuntu 10.04 virtual , without using DHCP server ?

Part Number: TMS320DM8168

Tool/software: Linux

Hello , 

I install ti-ezsdk_dm816x-evm_5_05_02_00 on ubuntu 10.04 . 

Now i want to boot from tftp and nfs server with Static IP . 

because when i wanna use DHCP3-server on ubuntu 10.04 , it can't start properly and Failed ! 

Here is my Bootargs command :

bootargs=console=tty02,115200 ip=dhcp root=/dev/nfs rw nfsroot=192.168.1.1:/home/dvr/targetfs mem=258M earlyprintknotifyk.vpssm3_sva=0xBF900000 vram=50M ti816xfb.vram=0:16M,1:16M,2:6M rootdelay=4

is it correct ?

how can do it ?

  • Hi Ehsan,

    Ehsan Hemati said:
    Now i want to boot from tftp and nfs server with Static IP . 

    Ehsan Hemati said:
    ip=dhcp

    For booting with static IP, you boot arguments are NOT correct. Please check the below e2e thread for more details of static IP configuration.

    Regards,
    Pavel