This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TCI6638K2K: TCI6638K2K- DDR3A and DDR3B

Part Number: TCI6638K2K

Tool/software: Code Composer Studio

Hello,

In the K2H_K2EVM-HK_SCH_REV4P0_1104 schematics , TI SOC is powered by VCCA0V75REF for DDR3AVREFSSTL (pin G14) and VCCB0V75REF powers DDR3BVREFSSTL (pin AC31).

Is there any requirement to power it using separate rails VCCA0V75REF and VCCB0V75REF? Why can't is be powered from same rail if current is the only concern? 

Is there anything like both DDR3 channels of the SOC have to be powered separately? or can it be combined?

Please comment.

Thanks,

Vidhya