Part Number: TMS320C6670
Tool/software: Code Composer Studio
I am using TMS320C6670 to perform LTE PDSCH with BCP.
In the example project, we changed the input data to 40 bits and TBS to 40.
I inserted the same input data in matlab.
It is not appropriate to compare the result of matlab with the result of BCP CRC.
I know what a little endian way is. However, apart from that, the result itself is not correct.
I want to know why.
Input data -> 0x253b1447, 0x70 So 40-bit
BCP result -> 0x47, 0x14, 0x3b, 0x25, 0x70, 0xee, 0x3e, 0x30
The matlab result is different from the above BCP result.
And I wonder in what order the 32-bit information bits in hexadecimal numbers go in order.
I would appreciate your reply.