Part Number: BEAGLEBK
Good morning,
I'm trying to update to start beagleBone black from SD card, concerning this I've installed on the SD CARD
Debian 9.1 2017-08-31 4GB SD LXQT image from http://beagleboard.org/latest-images
I've formatted the SD-CARD with HPUSBDisk-2.2.3.exe
and written the image with Win32DiskImager
I've followed the procedure:
0) remove power and/or usb connection
1) insert the SD CARD
2) Hold S2 button and insert power plug
the result is that the four led never flash as described, on the debug connector I can see a long long long sequence of "C" characters.
It seems to me that the sd-card reader is broken, how can I check this?
I've no problem when starting from eMMC but I want to change the image on the eMMC and it seems not possible.
Thanks
Antonio