Part Number: AM5718
Tool/software: Linux
Dear team,
I run the GateMP example for long time.The example protect share memory using the GateMP between A15 and DSP,but sometime it can not protect.
I follow the linux code GateHWSpinlock.c.
In GateHWSpinlock_start
---------------------------------------------------------------------
/* Fall back to /dev/mem if hwspinlock_user driver is not supported */
Mod->fd = open("/dev/hwspinlock", O_RDWR);
if (Mod->fd < 0) {
Mod->fd = open ("/dev/mem", O_RDWR | O_SYNC);
}
else {
Mod->useHwlockDrv = true;
}
-----------------------------------------------------------------
The /dev dictionary does not have spinclock device, use /dev/mem?
I see page 5421 of the spruhz7f.pdf. It said "A spinlock should only be held with interrupts disabled."
But in function GateHWSpinlock_enter
---------------------------------------------------------------
IArg GateHWSpinlock_enter(GateHWSpinlock_Object *obj)
{
volatile UInt32 *baseAddr = Mod->baseAddr;
struct hwspinlock_user_lock data = {
.id = obj->lockNum,
.timeout = 10,
};
IArg key;
Bool locked;
key = IGateProvider_enter(obj->localGate);
/* if gate already entered, just return with current key */
obj->nested++;
if (obj->nested > 1) {
return(key);
}
/* enter the spinlock */
while (1) {
if (Mod->useHwlockDrv) {
locked = !ioctl(Mod->fd, HWSPINLOCK_USER_LOCK, &data);
}
else {
/* read the spinlock, returns non-zero when we get it */
locked = (baseAddr[obj->lockNum] == 0);
}
if (locked) {
break;
}
obj->nested--;
IGateProvider_leave(obj->localGate, key);
key = IGateProvider_enter(obj->localGate);
obj->nested++; /* re-nest the gate */
}
return (key);
}
---------------------------------------------------------------
The function IGateProvider_enter use the pthread_mutex_lock.
I am not find the operation to disable interrupt.
Does the code really make sure the hwspinlock work properly?
Here is my error log.
--> main:
CMEM_init success
--> Main_main:
--> GateMPApp_create:
GateMPApp_create: Host is ready
<-- GateMPApp_create:
--> GateMPApp_exec:
GateMPApp_exec: Using host-created gate
GateMPApp_exec: Using slave-created gate
GateMPApp_exec: unexpected variable value.Test failed.
GateMPApp_exec: Previous value: 518, c[ 3647.514352] omap_hwmod: mmu1_dsp1: _wait_target_disable failed
urrent value=1
<-- GateMPApp_exec: -268435456
<-- Main_main:
[ 3647.527235] omap_hwmod: mmu0_dsp1: _wait_target_disable failed
<-- main: