Part Number: AM3352
Hello:
We do the DDR SI test by Agilent Oscilliscope.
Test results show that SRQdiffR and SRQdiffF are failed.
According to JEDEC definition, the value should between 5 to 10V/ns. Ours result is a little bit than 5V/ns.
After check user manual of AM335x, there are some registers can adjust slew rate of DQS:
1404h ddr_cmd0_ioctrl Section 9.3.1.87
1408h ddr_cmd1_ioctrl Section 9.3.1.88
140Ch ddr_cmd2_ioctrl Section 9.3.1.89
1440h ddr_data0_ioctrl Section 9.3.1.90
1444h ddr_data1_ioctrl Section 9.3.1.91
(according to the datasheet, I use the same value for all these registers, I change slew rate only, and also both slew rate and output impedance. Default value in our FW is 0x183, I change to 0x83, then 0xE3)
but after change register value to highest, no changes in the waveform.
Could you help to check, if we want to change slew rate of DQS, by modifying of registers above is enough or not?
Thanks