Part Number: AM1705
Tool/software: Linux
hello,
I'm using "AM1705" at the moment, on which Linux version "2.6.33" OS is running. I created ramdisk file by myself hence might be possible I'm missing so many important files. I have connected my SDCARD to the "MMCSD" port. so I want to know how can I access or use SDCARD for file writing and reading purpose at UI level[command line interface].
as I'm not very familiar with Linux OS and its's interface mechanism so I request you to guide me with as smallest details as possible. also, I'm having some doubt like whether it will appear as the interfaced device in /root/dev or as like normal directory in the particular folder which we can access using file system[similar to HDD interface in PC system eg: root/media/HDDname].
are there any sample codes or link which I can refer to understand the function and working principle in a better way.
thanks and regards.
f.khan