Part Number: TMS320C6674
Other Parts Discussed in Thread: TMS320C6678,
Tool/software: Code Composer Studio
First question
I have a question about EMAC on the TMS320C6678.
I remember that using the two Ethernet ports in the MCSDK was a problem.
Did the upgraded PROCESSOR RTOS SDK resolve this issue?
Second question
We are going to make a board with TMS320C6674.
However, this board should use Ethernet 2 port.
One port connects the Ethernet PHY to the transformer.
The other port directly connects the SERDES SGMII without PHY.
Is there any problem with this configuration using NDK?
Can NDK be used on ports without PHY?