Part Number: TMS320C6678
Tool/software: Code Composer Studio
CCS version:7.2.0.00013
Example location: in the folder ti\pdk_c667x_2_0_7\packages\ti\drv\srio\test\tput_benchmarking
Problem:When I am running the example in the c-s-c or the b-s-b mode .It will show the debug message "the srio port 0 is not operational." and the program will soon fall in an endless loop(in the latencytest),not typing anything.This dosen't happen in the c-i-c mode or the b-e-b mode.The srio switch is probably set already by ARM and the srio id is also adjusted.