This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux: Memory mapping different in windows and linux compiled code.



Tool/software: Linux

Hi,

I have my code base checked out on both Linux and Windows. I have ported the code compilation from windows to linux.

The following tools are used for compilation (both in windows as well as linux)
DSP_BIOS: 5.33.03.00
C6000_CGT: 6.1.11
TI_CSL: c6488

There are no additional optimizations done on linux.

Yet there are some differences in the memory mapping. I have attached the map files for your reference.
Could you please help me figure out why the differences are seen in the memory placements?

Thanks,

Tejaswini

meswtrx_core0_map_LINUX.txtmeswtrx_core0_map_WINDOWS.txt