Part Number: DRA756
Other Parts Discussed in Thread: DRA77P
Tool/software: Linux
Hi,
we are using PSDKLA 3.04.00.03 on a custom board with following EMIF setup:
2GB DDR3L RAM, of which 1GB connected to EMIF1 with additional chip for ECC and 1GB to EMIF2.
I saw that ECC support has been introduced in u-boot 2017.01 branch ( commit at omapzoom.org/ ) but hasnn't been merged in current PSDKLA u-boot.
Questions:
- how can we enable ECC on current PSDKLA? Is sufficient to backport ECC patches on 2017.01 u-boot branch?
- since we only need a part of ECC-protected memory, I would adopt the following LISA setup:
+ 512MB non-interleaved memory on EMIF1, ECC-protected
+ 1GB interleaved memory (EMIF1 + EMIF2)
+ last 512MB non-interleaved memory on EMIF2
Is this possible / make some sense? Can you suggest a suitable LISA mapping?
Thank you
Regards,
Francesco