Part Number: PRU-SWPKG
Other Parts Discussed in Thread: PRU-CGT
Tool/software: Linux
I am following the "PRU-Training: Hands-On Labs" guide to try to program the PRU in the Beaglebone Black.
I am trying the "LAB 1", and until the step 7 everything compiles and works fine. But i can't move to the step 8 because i do not have neither a JTAG emulator nor a FTDI cable.
How can i load a program to the AM335X of the Beaglebone Black without using the JTAG emulator and a FTDI cable? What files must be copied to the BBB?
Any help in the form of either a tutorial or a step-by-step guide would be very helpful, since most of the information in the internet seems to be outdated (e.g.: the directory '/sys/devices/bone_capemgr.?/slots' was moved to '/sys/devices/platform/bone_capemgr/slots') or the tools used are not well documented.
Hardwares:
OS: Debian 9.2 2017-10-10 4GB SD IoT
Kernel: Linux beaglebone 4.4.84-ti-r120
Board: Beaglebone Black, connected through SSH
Softwares:
CCS7.4.0.00015_linux-x64
PRU-CGT 2.2.1
PRU Software Support Package 5.0