This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reg: possibility of reading more than 16 bytes in UART Rx buffer

Other Parts Discussed in Thread: TMS320DM6437

Hi,

Topic: ZMODEM protocol implementation

Server: Tera Term Professional, Version 4.56.

Client: DAVINCI TMS320DM6437 EVM

When I send ZRQINIT Init. command (24 bytes of data) from server to client,

Client's Receive buffer (RBR) is able to receive only 16 Bytes of data instead of 24 bytes long data.

Receive Buffer (RBR) is 16 Byte FIFO. Is it possible to receive remaining 8 bytes of data,

If yes, Please suggest me how to do.

Thanks in advance,

Regards,

P. Sivachandran.