This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: eMMc does not work well after boot

Part Number: TMS320C6748

Hi !

In my work,C6478 boot whit eMMc.It works well with a simple led shinng program.

And then I try to boot with a emmc program.

After boot,emmc program stoped when reading the ext_csd information from emmc card. The status is  timeout.

	status =  SDMMC_sendCmd(hSDMMCMemInfo->hSDMMCInfo, 0x2000 |SDMMC_CMD8|SDMMC_RSP1,0, 0xFFFF);
	if( status != E_PASS )
	{
		asm(" SWBP 0 ");
	}

I can not read or write emmc after boot .

The program works well in CCS Debug.But it failed when boot from emmc.

The emmc version is 5.0.I flash the program at the 3rd sector of emmc.

thanks!