This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

configuration of hardware interruprs (HWI) and DSP/BIOS 5.41

Hi,

 

I am having trouble finding a comprehensive list of predefined hardware interrupts HWIs for the VC5505 using DSP/BIOS 5.41. Basically would like to setup 2 DMA chanels for audio transfer from an AIC3204 codec, but using DSP/BIOS. It has been mentioned that HWI_8 is predefined for DMA use but this is not immediately obvious in the BIOS configuration tool. Is there an app note that discusses this very use of DSP/BIOS for DMA use ? Unfortunately none of the BIOS examples treat this HWI configuration thoroughly (as far as I can tell). Would appreciate some guidance on this task ...

Regads, M