Other Parts Discussed in Thread: OMAP3530
Hi,
Two questions regrading Power
1. i am interfacing with a 5V SPI slave, can i connect the OMAP3530 directly to him or do i need to somehow pull voltage up (if yes how so?, pull up resistor?, driver?)
2. what is the maximum voltage i can output from a GPIO?, from what i have read it is 3.3V but would like to be sure
Thanks in Advanced and
Best Regards,
Ran.