Part Number: DRA722
Hi all,
Im using a custom board based on DRA722 .I'm not able to boot from QSPI flash if I turn OFF the debug messages.But with debug printing turned ON,Im able to boot successfully.Now I have configured qspi flash to run at 8MHz.If use higher frequencies,that also leads to failure.
What could be the reason?
QSPI FLASH part number:mt25ql02gc
Regards,
Murugan S