Part Number: DRA756
Hi,
I am investigating using the DRA75x timer PWM outputs (in toggle mode) for secondary system clocks in the 500kHz to 2MHz range. These signals ideally need to be fairly low jitter (<=1nS). The assumption is that the timer outputs will be synchronous to the L4 Peripheral clock. So looking for any information regarding jitter of these outputs. For example, if using sysclk1 at 20.0MHz as a clock source to the timer, and L4 peripheral clock is at 133MHz, will the timer output be subjected to 7.5nS of jitter (1/133.3MHz)?
Thanks,
Eric