Part Number: TMS320C6678
Tool/software: Code Composer Studio
we use BCM5464 PHY chip
We modify GE.pjt from K1_STK_v1.1.rar package, and it runs ok:
JTAG ID= 0x1009e02f. This is C6678/TCI6608 device, version variant = 1.
DEVSTAT= 0x0000d40d. little endian, SPI boot, PLL configuration implies the input clock for core is bypassed.
SmartReflex VID= 63, required core voltage= 1.104V.
Die ID= 0x0b00f009, 0x0404251b, 0x00000000, 0x59ce0021
Device speed grade = 1250MHz.
Enable Exception handling...
Initialize DSP main clock = 312.50MHz/1x4 = 1250MHz
Initialize PASS PLL clock = 100.00MHz/2x21 = 1050.000MHz
Initialize DDR speed = 312.50MHzx/5x26 = 1625.000MTS
GE auto negotiation (master) two DSPs test (DSP0 -> DSP1)...
link PHY1 is NOT up
Transferred 3000 bytes with 10001310 cycles, throughput= 2Mbps.
number of descriptors in host queue DDR_HOST_SIZE0_FDQ (2058) changed from 512 to 518
0x82340041->0x82340061->0x82340081->0x823400a1->0x823400c1->0x823400e1->0x82340101->0x82340121->0x82340141->0x82340161->...
STATSA.RxGoodFrames =8
STATSA.RxOctets =12144
STATSA.Frame1024tUp =8
STATSA.NetOctets =12144
STATSB.TxGoodFrames =8
STATSB.TxOctets =12144
STATSB.Frame1024tUp =8
STATSB.NetOctets =12144
SGMII0 Link Partner Advertised Ability 10Mbps Half Duplex
SGMII1 Link Partner Advertised Ability 10Mbps Half Duplex
MDIO ALIVE flag: 0x0000000c
MDIO LINK flag: 0x0000000c
GE test complete.
Then we run helloWorld.pjt. Because giganet is already configured, we set sFlags.phy (in EVM_init() function) from 1 to 0.
The board is directly connected to my PC net port. A program on my computer sends data to C6678 board. It can work, but the speed is about 6MB/s. The property of my PC netport is 1Gbps.
Why is the speed very low?
Thanks!