Hi to all,
I want to switch the video output to digital RGB 565 or 888 with 480 x 272 resolution in "v4l2 example" runnig on DM6446EVM . Although I changed the parameter in "video.conf" for that example to output 640x480 LCD output , I think that it is YCbCr output.
How can I configure the parameters
1- Video output color space type (YUV, RGB)
2- Resolution of the video displayed
3- LCD timing parameters
I read the document "Digital Video Using DaVinci SoC" (SPRAAN0) but it is not for SDK v1.30. Is there any new version of that document ?
Ferhat