Part Number: AM4376
Other Parts Discussed in Thread: AM4372
Tool/software: Linux
Hello,
we use mainline kernel 4.9.61 with RT-patch on a custom board with AM4376.
The goal is to use PRU: all 4 cores (without PRU ETH)
So I have ported the PRU related stuff from TI BSP: am437x-evm-linux-rt-sdk-src-04.02.00.09
Here the dmesg output at the start of PRU subsystem:
[ 87.545684] ti-pruss 54400000.pruss: creating PRU cores and other child platform devices [ 87.582027] ti-pruss 54440000.pruss: creating PRU cores and other child platform devices [ 88.085916] pru-rproc 54434000.pru0: memory iram: pa 0x54434000 size 0x3000 va e0b2c000 [ 88.085950] pru-rproc 54434000.pru0: memory control: pa 0x54422000 size 0x400 va e0b5d000 [ 88.085965] pru-rproc 54434000.pru0: memory debug: pa 0x54422400 size 0x100 va e0b5f400 [ 88.085982] pru-rproc 54434000.pru0: mbox_request_channel failed: -19 [ 88.091492] remoteproc remoteproc0: 54434000.pru0 is available [ 88.091625] pru-rproc 54434000.pru0: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@54400000/pru@54434000 probed successfully [ 88.093318] pru-rproc 54438000.pru1: memory iram: pa 0x54438000 size 0x3000 va e0b64000 [ 88.093365] pru-rproc 54438000.pru1: memory control: pa 0x54424000 size 0x400 va e0b61000 [ 88.093382] pru-rproc 54438000.pru1: memory debug: pa 0x54424400 size 0x100 va e0b68400 [ 88.093394] pru-rproc 54438000.pru1: mbox_request_channel failed: -19 [ 88.097845] remoteproc remoteproc1: 54438000.pru1 is available [ 88.099976] pru-rproc 54438000.pru1: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@54400000/pru@54438000 probed successfully [ 88.101376] pru-rproc 54474000.pru0: memory iram: pa 0x54474000 size 0x1000 va e0b6a000 [ 88.101424] pru-rproc 54474000.pru0: memory control: pa 0x54462000 size 0x400 va e0b6c000 [ 88.101440] pru-rproc 54474000.pru0: memory debug: pa 0x54462400 size 0x100 va e0b6e400 [ 88.101453] pru-rproc 54474000.pru0: mbox_request_channel failed: -19 [ 88.108919] remoteproc remoteproc2: 54474000.pru0 is available [ 88.111589] pru-rproc 54474000.pru0: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@54440000/pru@54474000 probed successfully [ 88.112675] pru-rproc 54478000.pru1: memory iram: pa 0x54478000 size 0x1000 va e0b70000 [ 88.114844] pru-rproc 54478000.pru1: memory control: pa 0x54464000 size 0x400 va e0b72000 [ 88.114869] pru-rproc 54478000.pru1: memory debug: pa 0x54464400 size 0x100 va e0b74400 [ 88.114887] pru-rproc 54478000.pru1: mbox_request_channel failed: -19 [ 88.118688] remoteproc remoteproc3: 54478000.pru1 is available [ 88.122896] pru-rproc 54478000.pru1: PRU rproc node /ocp@44000000/pruss_soc_bus@54426000/pruss@54440000/pru@54478000 probed successfully
It seems to be the device tree issue (see /drivers/mailbox/mailbox.c):
struct mbox_chan *mbox_request_channel(struct mbox_client *cl, int index)
{
struct device *dev = cl->dev;
struct mbox_controller *mbox;
struct of_phandle_args spec;
struct mbox_chan *chan;
unsigned long flags;
int ret;
if (!dev || !dev->of_node) {
pr_debug("%s: No owner device node\n", __func__);
return ERR_PTR(-ENODEV);
}
mutex_lock(&con_mutex);
if (of_parse_phandle_with_args(dev->of_node, "mboxes",
"#mbox-cells", index, &spec)) {
dev_dbg(dev, "%s: can't parse \"mboxes\" property\n", __func__);
mutex_unlock(&con_mutex);
return ERR_PTR(-ENODEV);
}
Here is our dts patch:
diff -urwN a/arch/arm/boot/dts/am4372.dtsi b/arch/arm/boot/dts/am4372.dtsi
--- a/arch/arm/boot/dts/am4372.dtsi 2018-01-03 08:26:14.553435200 +0100
+++ b/arch/arm/boot/dts/am4372.dtsi 2018-01-10 09:44:20.312435400 +0100
@@ -342,6 +342,14 @@
ti,mbox-tx = <0 0="">;
ti,mbox-rx = <0 0="" 3="">;
};
+ mbox_pru1_0: mbox_pru1_0 {
+ ti,mbox-tx = <2 0="">;
+ ti,mbox-rx = <3 0="">;
+ };
+ mbox_pru1_1: mbox_pru1_1 {
+ ti,mbox-tx = <4 0="">;
+ ti,mbox-rx = <5 0="">;
+ };
};
timer1: timer@44e31000 {
@@ -926,6 +934,140 @@
interrupts = <GIC_SPI 111 IRQ_TYPE_LEVEL_HIGH>;
};
+ pruss_soc_bus: pruss_soc_bus@54426000 {
+ compatible = "ti,am4376-pruss-soc-bus";
+ reg = <0x54426000 0x2000="">;
+ ti,hwmods = "pruss";
+ #address-cells = <1>;
+ #size-cells = <1>;
+ ranges;
+ status = "disabled";
+
+ pruss1: pruss@54400000 {
+ compatible = "ti,am4376-pruss";
+ reg = <0x54400000 0x2000="">,
+ <0x54402000 0x2000="">,
+ <0x54410000 0x8000="">,
+ <0x54426000 0x2000="">,
+ <0x5442e000 0x31c="">,
+ <0x54432000 0x58="">;
+ reg-names = "dram0", "dram1", "shrdram2", "cfg",
+ "iep", "mii_rt";
+ #address-cells = <1>;
+ #size-cells = <1>;
+ ranges;
+ status = "disabled";
+
+ pruss1_intc: intc@54420000 {
+ compatible = "ti,am4376-pruss-intc";
+ reg = <0x54420000 0x2000="">;
+ reg-names = "intc";
+ interrupts =
+ <GIC_SPI 20 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 21 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 22 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 23 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 24 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 26 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 27 IRQ_TYPE_LEVEL_HIGH>;
+ interrupt-names = "host2", "host3",
+ "host4", "host5",
+ "host6", "host8",
+ "host9";
+ interrupt-controller;
+ #interrupt-cells = <1>;
+ };
+
+ pru1_0: pru@54434000 {
+ compatible = "ti,am4376-pru";
+ reg = <0x54434000 0x3000="">,
+ <0x54422000 0x400="">,
+ <0x54422400 0x100="">;
+ reg-names = "iram", "control", "debug";
+ label = "pru0";
+ interrupt-parent = <&pruss1_intc>;
+ interrupts = <16>, <17>;
+ interrupt-names = "vring", "kick";
+ status = "disabled";
+ };
+
+ pru1_1: pru@54438000 {
+ compatible = "ti,am4376-pru";
+ reg = <0x54438000 0x3000="">,
+ <0x54424000 0x400="">,
+ <0x54424400 0x100="">;
+ reg-names = "iram", "control", "debug";
+ label = "pru1";
+ interrupt-parent = <&pruss1_intc>;
+ interrupts = <18>, <19>;
+ interrupt-names = "vring", "kick";
+
+ status = "disabled";
+ };
+ };
+
+ pruss0: pruss@54440000 {
+ compatible = "ti,am4376-pruss";
+ reg = <0x54440000 0x1000="">,
+ <0x54442000 0x1000="">,
+ <0x54466000 0x2000="">,
+ <0x5446e000 0x31c="">,
+ <0x54472000 0x58="">;
+ reg-names = "dram0", "dram1", "cfg",
+ "iep", "mii_rt";
+ #address-cells = <1>;
+ #size-cells = <1>;
+ ranges;
+ status = "disabled";
+
+ pruss0_intc: intc@54460000 {
+ compatible = "ti,am4376-pruss-intc";
+ reg = <0x54460000 0x2000="">;
+ reg-names = "intc";
+ interrupts =
+ <GIC_SPI 159 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 160 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 161 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 162 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 163 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 164 IRQ_TYPE_LEVEL_HIGH
+ GIC_SPI 165 IRQ_TYPE_LEVEL_HIGH>;
+ interrupt-names = "host2", "host3",
+ "host4", "host5",
+ "host6", "host8",
+ "host9";
+ interrupt-controller;
+ #interrupt-cells = <1>;
+ };
+
+ pru0_0: pru@54474000 {
+ compatible = "ti,am4376-pru";
+ reg = <0x54474000 0x1000="">,
+ <0x54462000 0x400="">,
+ <0x54462400 0x100="">;
+ reg-names = "iram", "control", "debug";
+ label = "pru0";
+ interrupt-parent = <&pruss0_intc>;
+ interrupts = <16>, <17>;
+ interrupt-names = "vring", "kick";
+ status = "disabled";
+ };
+
+ pru0_1: pru@54478000 {
+ compatible = "ti,am4376-pru";
+ reg = <0x54478000 0x1000="">,
+ <0x54464000 0x400="">,
+ <0x54464400 0x100="">;
+ reg-names = "iram", "control", "debug";
+ label = "pru1";
+ interrupt-parent = <&pruss0_intc>;
+ interrupts = <18>, <19>;
+ interrupt-names = "vring", "kick";
+ status = "disabled";
+ };
+ };
+ };
+
mcasp0: mcasp@48038000 {
compatible = "ti,am33xx-mcasp-audio";
ti,hwmods = "mcasp0";
In my opinion "mboxes" statement is missing. But in which shape ?
Please help us to integrate PRU.
P.S.: I didn't test it with TI board and BSP, but I think the problem is there also present.
Best regards
Walter Wagner ABB