Other Parts Discussed in Thread: OMAP3503
I'm working with a design which may potentially connect many devices to the GPMC bus on the OMAP3503. To make sure the processor can handle this design I'm looking through the 3503 data sheet trying to learn what he maximum load capacitance and drive strength of the GPMC bus pins are. In the SPRS505 data sheet in section 6 it lists Cload as 15pF. That seems extremely low though it doesn't list it as the "Max" value, it just lists it as the value used for testing. Can you point me at some documentation that describes the maximum load capacitance for the GPMC address and data lines?
Thank you,
Jemiah
.