This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/66AK2H14: RTOS/66AK2H14

Part Number: 66AK2H14

Tool/software: TI-RTOS

Hi

I am using 66AK2H14 processor and pdk_k2hk_4_0_7.

I have to verify all the 4 SGMII ports in non Loop Back mode.Is there any example in pdk which does the same???

I have gone through the drv/pa/example/multicoreExample/src/multicore_example.c example and I found that only 2 MAC ports are used in non Loop Back mode.

whether I can change the number of mac ports to 4 in the same code ?? Is there any limitation for that??

Please help me with this.

Thanks and Regards,

Mahima Shanbag