Part Number: TMS320C6713B
Other Parts Discussed in Thread: CCSTUDIO
Tool/software: Code Composer Studio
Hello everyone,
I have started working on DSP processor, my college have provided me TMS320C6713 DSK board. The CD provided by TI contains all the software for Windows XP system, but when I installed the softwareon the system and started the C6713 DSK diagnosis the application showing 'FAIL' message. USB emulation is failed. The mistake which I think I have done is that I have installed the software by connecting the board and installing the software. I have removed the software and again installed the software but this time I have removed the USB, still the diagnosis fails. What should I do now?
My another problem is when I was running the CCStudio v3.1 the examples are running properly, means the LED exapmple etc. but when I have copy and pasted the same code into a new project file the code is showing lot of error message. The things I have copied are the .c file, .cmd file. few errors are rectified when I have removed the header.
Again I have tried to write the code this time I was taking the help of book and writing the code as written in the book. created the .c file .cmd file but again the compilation error.
I am not getting how to write the code in the CCStudio what are steps that I am missing here I am not getting. I am comfortable in using KEIL uVision. But this software is very different and difficult to use.
I have installed matlab 2009a on the system, but the c6000 toolbox is missing, how to download that toolbox and also is there any issue regarding the matlab coding to board that I have to keep in mind.
Please guide me and resolve my issue.
Thank you.
My email: shahrukh.md1995@gmail.com
Please If possible then guide me personally