This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flashing the UBL to NOR flash without RBL UART boot

I have a custom board with the DM6467. I am also running ccsv4. I've checked out the board and DDR2 and NOR flash working properly. Since our board is configured for EMIFA NOR boot (resistors hardwired), how can I flash the UBL to the NOR easily from ccsv4 or other means? I don't have the RBL UART boot configuration easily available to me without re-soldering some resistors to change the configuration.

I have compiled the UBL and converted to .bin using hex470.exe and ascii2bin.exe...