Part Number: TMDSCSK388
Other Parts Discussed in Thread: DM388
TMDSCSK388 purchased at Ti Store, order no. 1682548.
1、According to the User Guide, the TMDSCSK388 is set up。In TeraTerm after setting the serial port option, Boot up is not happening its showing " CCCCCCCC " continues in Teraterm window。 No boot up and No signal from HDMI port。
2、The prebuilt binaries from the IPNC RDK 3.9.1 package is flashed on the new micro-SD , Re-create SD card, not solve the issue also。
3、Rebuild the software with DM388 option set in Rles.make file sysclean & sysall to build ,Re-create SD card, not solve the issue also。