This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: 9-bit UART

Part Number: AM3358


I'm looking to deploy an AM3358 into a new application, but one of the issues is the need to handle 9bit serial through the UART, rather than the usual 8bit. On other lower-end devices, eg the TM4C, their supported UART has a special 9bit mode, but it doesn't look like this is available on the Sitara.

Has anyone successfully implemented 9bit serial, or can anyone suggest a suitable way to do it (short of bouncing through a Tiva first)? I'm wondering whether the processor might just be fast enough to accommodate 8bit+1bit transfers, or whether theres something simple which can be done in the PRU?

cheers

Mat