Part Number: OMAP-L138
Other Parts Discussed in Thread: TMDSLCDK138, OMAPL138
Tool/software: Linux
Hi,
Recent, I was learning how to boot linux system from MMCSD. My hardware is TMDSLCDK138, the SD card is 8GB. I downloaded the .img(omapl138-lcdk-linux-04.02.00.09.img), and win32diskimager, I followed this link to flash MMCSD http://processors.wiki.ti.com/index.php/Processor_SDK_Linux_Creating_a_SD_Card_with_Windows. There was two partitions in the SD, one is fat, and I can see "u-boot-omapl138-lcdk.ais" in the fat partition. I switched the DIP to "0001" , and I opened Tera Term, the baud is 115200. There was nothing in the Tera Term screen. Could you tell me how to make SD card that can boot linux.
Thank you very much.
Best regards.
Ruddy