This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: No debug output after power-up

Part Number: AM5728

Tool/software: Linux

Hi,ti experts,our custom board based on AM5728 IDK reference.we make the uboot and image to the sd card and insert it into the sd card slot,connect the cable with uart3,the minicom config as follow graph,

we config the SYSBOOT pins:SYSBOOT5=1  SYSBOOT4=0 SYSBOOT1=1 SYSBOOT0=0,and the other pin are 0, which means boot sequence by the TRM as follow picture by red box:

after then we power up the board,there's no information ouput on the minicom.we test all kinds of voltage output by power ic are nomal,and the sd card cd pin is 0v.is there some place we do wrong?