I have used "dv_flasher.exe" to write u-boot image to a NAND (MT29F2G08ABD) through serial port. UBL runs but gives message like NAND timeout. Thus NAND booting is failing. I have toggled the switches to boot from NAND but still there is no boot message. Do I need to recompile " dv_flasher.exe" by doing NAND specific changes or is there any problem with the EMIF bus?
Flashing of NAND through CCS (flashwriter_nand.out) is also failing as I do not get any dialog asking for "ubl_nand.bin". I am using CCS version 3.3.