This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSP/BIOS crashing



Hi,

I am using EVM 6474 and DSP/BIOS, and my application runs on CORE0.

I have three interrupts configured,

1. Mcbsp Receive ready interrupt.

2. Gpi interrupt

3. IPC interrupt.

When I enable the PRD module (i.e. Use CLK Manager to run PRD), the core 0 crashes and goes to Exception handler.

below is my observation on Message LOG,

=============================

817 TSK: running dynamic TSK (0x008018dc)

818 SWI: end KNL_swi (TSK scheduler) (0x874e10) state = done

819 CLK: current time = 125 (0x0000007d)

820 PRD: tick count = 125 (0x0000007d)

821 SWI: post KNL_swi (TSK scheduler) (0x874e10)

822 SWI: begin KNL_swi (TSK scheduler) (0x874e10)

823 EXC_exceptionHandler: EFR=0x2

824 NRP=0x10000

825 mode=supervisor

========================================

but. when i disabled PRD module from using the CLK Manager, It is working fine.

can u please help me on this.?

 

Thanks,

Bala