Part Number: AM3715
So in this application we have cvideo1_vfb and Cvideo1_out tied together with a 2700 ohm resistor but the output is not connected to any composite connector. Normally we have cvideo1_rset tied to ground through a 4700 ohm resistor. So the set-up is ready for a s-video dc coupled high fs swing OR composite, DC coupled high FS swing but the output is not tied to a composite connector. On some of our units Rset did not get populated due to an error and what we are trying to figure out is if Rset is floating and video cvideo1_Vfb and cvideo1_out are looped together is there going to be any problems?