Part Number: DRA72XEVM
Other Parts Discussed in Thread: DRA742, PMP, DRA752, TVP5158
Tool/software: Linux
HI
could you please guide me to configure wayland/weston on the J6 board with a LCD. Following errors are what I got when I try to start weston.
root@dra7xx-evm:/opt/vision_sdk# weston
Date: 2017-03-09 UTC
[02:26:31.827] weston 1.9.0
http://wayland.freedesktop.org
Bug reports to: bugs.freedesktop.org/enter_bug.cgi
Build: 1.8.93-2-gb05cdb8 configure.ac: bump to version 1.9.0 for the official release (2015-09-21 18:11:26 -0700)
[02:26:31.827] OS: Linux, 4.4.45-00014-g14ab8c1-dirty, #29 SMP PREEMPT Fri Jan 12 15:22:16 CST 2018, armv7l
[02:26:31.828] Using config file '/etc//weston.ini'
[02:26:31.828] Loading module '/usr/lib/weston/drm-backend.so'
[02:26:31.832] Output repaint window is 30 ms maximum.
[02:26:31.832] initializing drm backend
[02:26:31.832] failed to get VT mode: Inappropriate ioctl for device
[02:26:31.832] fatal: drm backend should be run using weston-launch binary or as root
[02:26:31.832] fatal: failed to create compositor backend
root@dra7xx-evm:/opt/vision_sdk# weston-flower
failed to connect to Wayland display: No such file or directory
failed to create display: No such file or directory
root@dra7xx-evm:/opt/vision_sdk#
root@dra7xx-evm:/opt/vision_sdk# cat /etc/weston.ini
[core]
backend=drm-backend.so
idle-time=0
repaint-window=30
shell=ivi-shell.so
[ivi-shell]
ivi-module=ivi-controller.so
ivi-input-module=ivi-input-controller.so