Other Parts Discussed in Thread: TMS320DM6467
I'm trying to get through a morass of confusion with a lack of documentation. I'm writing this post to (1) ask for help from those leading the way, and (2) provide help to those following.
New project design. I need huge horsepower, so I'm looking at the DM6467T. I'd prefer to do digital HD video I/O, but have a compatibility need to analog SD video I/O. The digital HD part opens a bag of worms. I'm on an unbelievably short design cycle requirement (<2 months) for doing custom video analytics in the DSP.
QUESTION:
Starting from the Spectrum Digital HD1080p DVM, whose doc is pointed to by the TI DM6467T EVM and is presumably the same thing, I find that this EVM has composite and S-Video in (satisfying my analog SD video in need), plus Component video I/O (presumably providing HD video I/O, but in analog not digital). How easy or hard would it be, and how should I go about it, to add (A) Composite or S-Video OUT, and (B) DVI or HDMI video IN and OUT?
FOR OTHERS:
I found the TI doc "HDMI Transmitter/Receiver Support on TMS320DM6467" pdf at http://focus.tij.co.jp/jp/lit/an/spraav4/spraav4.pdf . It refers to SiI9134 and SiI9135, but only in a summary manner. SiI is http://www.siliconimage.com . Datasheets on these parts are NOT found on their website, and the SiI9134 seen in SiI9135 illustrations doesn't even exist on their website. Calling them and then Nu Horizons (distributor), I find it's about intellectual property. You have to sign an NDA before you can see the datasheet(s). (Note this doesn't help me for doing early evaluations at all.) Furthermore, since these HDMI chips include HDCP, you need some additional signing or licensing or something. This just erects more obstacles to investigating whether or not this is the direction to go at all.
I backed up to DVI, since I don't need HDCP or audio. Silicon Image has DVI chips. Great! I find a datasheet for the one DVI receive on their website, SiI1161. They seem to have three transmitters, and I'll have to do more investigation to pick one. Nevertheless, the fact that datasheets are available without all the admin IP gook, might steer me that way. (Another QUESTION: Will I be able to integrate as easily with these DVI chips as the TI pdf implies I might with the HDMI chips?)
At the moment, I'm thinking I'm going to be forced to do this incrementally. First, start with the HD1080p EVM as it is, including the wrong fit of the HD video in and ALL the video out. Port my DM6446 video analytics already developed on a security camera platform, and get it running on the new evm. Then reassess my final I/O path. Note that I have extreme size constraints, and already plan to use multiple boards. With that in mind, I may go ahead and design my own core board, which has distinctly reduced functionality and size requirements from the HD1080p. Along with that, and here comes some unwanted overhead in my tight schedule, develop a wrong-fit secondary or daughter board containing the details of the wrong-fit video I/O identical to the HD1080p. Next, cross my fingers, dig deeper in the pile of it, and then develop a revised secondary or daughter board containing correct-fit video I/O.
-Helmut