Part Number: AM5708
Tool/software: Linux
Hi,
I have AM5708 based custom board and I had released revision A of that with 1GB of RAM with 532Mhz DDR frequency. Now I have reduced the size of DDR from 1GB to 512 MB and all the other components are same. Just DDR is changed with 2 Chips of 512 to 2 Chips of 256. I have changed Row size and Page size and LISA register according to DDR datasheet and Device tree node for memory in kernel. But When I power up the Board it hangs at ** Starting kernel **
I have changed :
In file arch/arm/boot/dts/am570x-custom-board.dts
memory { device_type = "memory"; reg = <0x0 0x80000000 0x0 0x40000000>; /* 1024 MB */ }; And I tried to modify reg to "reg = <0x0 0x80000000 0x0 0x20000000>;"
In Board file I have changed Registers for DDR :
const struct emif_regs j6e_emif_2_regs_ddr3_532_mhz_1cs_dra_es1 = {
.sdram_config_init = 0x61851AB2,
.sdram_config = 0x61851AB2,
.sdram_config2 = 0x00000000,
};
I have tried to modify .sdram_config_init from "0x618522B2" to "0x61851AB2" and sdram_config from "0x618522B2" to "0x61851AB2"
const struct dmm_lisa_map_regs j6e_lisa_map_4G_x_2_x_2 = {
.dmm_lisa_map_0 = 0x0,
.dmm_lisa_map_1 = 0x0,
.dmm_lisa_map_2 = 0x0,
.dmm_lisa_map_3 = 0x80500100,
.is_ma_present = 0x1
};
Modified .dmm_lisa_map_3 from "0x80600100" to "0x80500100"
U-Boot SPL EDGE
DRA722-GP ES2.0
Trying to boot from MMC1
U-Boot: CONFIG_SYS_MMCSD_FS_BOOT_PARTITION 1 : u-boot.img
SPL: trying to load u-boot.img from secondry partition!!
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-00333-ge1198ea-dirty (Jan 17 2018 - 11:33:14 +0530)
CPU : DRA722-GP ES2.0
Model: TI AM5708 EDGE
Board: AM570x EDGE REV
Watchdog enabled
DRAM: 512 MiB
MMC: no pinctrl for sdr104
no pinctrl for ddr50
no pinctrl for sdr50
no pinctrl for sdr25
no pinctrl for sdr12
no pinctrl for hs200_1_8v
OMAP SD/MMC: 0, OMAP SD/MMC: 1
reading uboot.env
** Unable to read "uboot.env" from mmc0:1 **
Using default environment
SCSI: 0 device not found
ERROR: scsi device not found
at drivers/block/disk-uclass.c:43/scsi_init()
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
U-Boot: Loaded, undefined EEPROM reg value!!
Kernel: Secondary Fail, booting from primary kernel!!
FS : Booting from primary FS!!
Autoboot in 2 seconds
EDGE# setenv boot_fit 0
EDGE# boot
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
** Unable to read file uEnv.txt **
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading zImage
3738192 bytes read in 173 ms (20.6 MiB/s)
reading am570x-edge.dtb
85212 bytes read in 10 ms (8.1 MiB/s)
Kernel image @ 0x82000000 [ 0x000000 - 0x390a50 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe8000, end 8ffffcdb ... OK
Starting kernel ...
I have followed and changed accordingly but no luck :
https://e2e.ti.com/support/arm/automotive_processors/f/1020/t/651203
and
https://e2e.ti.com/support/arm/automotive_processors/f/1020/t/652269
Is there anything I am missing in configuration? I have Enabled Early printk from kernel also but there is no console log. I have Debugged spl via Jtag and I am able to write 512MB of (whole range) DDR via jtag.
Guide me in solving this problem.
Thank you,
Chintan.