Greetings,
I am using a XDS100 USB emulator from Olimex to try and connect to a DM6435. I have followed the installation instructions found at http://tiexpressdsp.com/wiki/index.php?title=XDS100 but cannot reset or connect.
I receive the following error on connect attempt: Error connecting to the target: Error 0x80000240/-151 Fatal Error during: Initialization, OCS, This error was generated by TI's USCIF driver. SC_ERR_POD_OPEN <-151> This utility failed to open the adapter for a custom emulator. The adapter returned an error.
I receive the following error on reset attempt: Failed to reset the emulator: This error was generated by TI's USCIF driver. SC_ERR_POD_OPEN <-151> This utility failed to open the adapter for a custom emulator. The adapter returned an error.
We have succesfully connected to this board using an XDS510 USB emulator. This is the first time we have used the XDS100 on any board. Thanks in advance for your help.
EDIT: After rebooting my PC the error on connect has changed to the following: Error connecting to the target: Error 0x80000240/-1146 Fatal Error during: Initialization, OCS, Invalid data was scanned by the emulation controller. Verify the board setup to make sure the scan chain is properly defined. If the setup is correct, then RESET EMULATOR. This will disconnect each target from the emulator. The targets should then be power cycled or hard reset followed by an emureset and reconnect to each target.
Fly