Hi All,
I am going to play back a voice by LCDK6748. everything is working well with the following code.
while(1) {
input = McASPRxBufRead(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_RX);
delay(500);
McASPTxBufWrite(SOC_MCASP_0_CTRL_REGS, MCASP_XSER_TX,input);
}
but, when I run with delay greater than 800, the code does not play anything. the delay is a symbol of a bunch of procedures. I need the code works with a much greater value of delay.
Can you help me to overcome this problem?
Regards