Part Number: AM5728
Other Parts Discussed in Thread: BEAGLEBOARD-X15, TLV320AIC3104
Tool/software: Linux
Hi ,
We are try to bring up the linux on AM5728 custom board with SDK 03.02.00.05.
it's throw some error and stop.
I attached the error log during the boot process.
Any one please help me to resolve this issue.
Thanks and Regards
U-Boot SPL 2016.05-g6c5519b6fc (Dec 14 2016 - 20:19:24) DRA752-GP ES2.0 Trying to boot from MMC1 reading args spl_load_image_fat_os: error reading image args, err - -1 reading u-boot.img reading u-boot.img reading u-boot.img reading u-boot.img U-Boot 2016.05-g6c5519b6fc (Dec 14 2016 - 20:19:24 -0500) CPU : DRA752-GP ES2.0 Model: TI AM5728 BeagleBoard-X15 Board: BeagleBoard X15 REV A.20 DRAM: 2 GiB MMC: no pinctrl for sdr104 no pinctrl for ddr50 no pinctrl for sdr50 no pinctrl for sdr25 no pinctrl for sdr12 OMAP SD/MMC: 0, OMAP SD/MMC: 1 reading uboot.env ** Unable to read "uboot.env" from mmc0:1 ** Using default environment SCSI: SATA link 0 timeout. AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst scanning bus for devices... Found 0 device(s). Net: Could not get PHY for ethernet@48484000: addr 1 Warning: ethernet@48484000 using MAC address from ROM eth0: ethernet@48484000 Hit any key to stop autoboot: 2 1 0 switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 reading boot.scr ** Unable to read file boot.scr ** reading uEnv.txt 574 bytes read in 3 ms (186.5 KiB/s) Loaded env from uEnv.txt Importing environment from mmc0 ... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 3597872 bytes read in 200 ms (17.2 MiB/s) 97618 bytes read in 25 ms (3.7 MiB/s) Kernel image @ 0x82000000 [ 0x000000 - 0x36e630 ] ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8ffe5000, end 8ffffd51 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Initializing cgroup subsys cpuset [ 0.000000] Initializing cgroup subsys cpu [ 0.000000] Initializing cgroup subsys cpuacct [ 0.000000] Linux version 4.4.32-gadde2ca9f8 (gtbldadm@ubuntu-16) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP PREEMPT Wed Dec 14 19:14:12 EST 2016 [ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache [ 0.000000] Machine model: TI AM5728 BeagleBoard-X15 [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000095800000, size 56 MiB [ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 64 MiB [ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created CMA memory pool at 0x000000009d000000, size 32 MiB [ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool [ 0.000000] Reserved memory: created CMA memory pool at 0x000000009f000000, size 8 MiB [ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool [ 0.000000] cma: Reserved 24 MiB at 0x00000000fe400000 [ 0.000000] Forcing write-allocate cache policy for SMP [ 0.000000] Memory policy: Data cache writealloc [ 0.000000] OMAP4: Map 0x00000000ffd00000 to fe600000 for dram barrier [ 0.000000] DRA752 ES2.0 [ 0.000000] PERCPU: Embedded 11 pages/cpu @eed33000 s14848 r8192 d22016 u45056 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 472640 [ 0.000000] Kernel command line: console=ttyO2,115200n8 root=PARTUUID=220d9257-02 rw rootfstype=ext4 rootwait [ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes) [ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes) [ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Memory: 1680588K/1897472K available (6579K kernel code, 360K rwdata, 2476K rodata, 332K init, 289K bss, 28468K reserved, 188416K cma-reserved, 1283072K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB) [ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc08e0044 (9057 kB) [ 0.000000] .init : 0xc08e1000 - 0xc0934000 ( 332 kB) [ 0.000000] .data : 0xc0934000 - 0xc098e2f0 ( 361 kB) [ 0.000000] .bss : 0xc0990000 - 0xc09d86c0 ( 290 kB) [ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1 [ 0.000000] Preemptible hierarchical RCU implementation. [ 0.000000] Build-time adjustment of leaf fanout to 32. [ 0.000000] NR_IRQS:16 nr_irqs:16 16 [ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div [ 0.000000] OMAP clockevent source: timer1 at 32786 Hz [ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns [ 0.000004] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns [ 0.000015] Switching to timer-based delay loop, resolution 162ns [ 0.000323] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns [ 0.000331] OMAP clocksource: 32k_counter at 32768 Hz [ 0.000737] Console: colour dummy device 80x30 [ 0.000752] WARNING: Your 'console=ttyO2' has been replaced by 'ttyS2' [ 0.000759] This ensures that you still see kernel messages. Please [ 0.000764] update your kernel commandline. [ 0.000777] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475) [ 0.000789] pid_max: default: 32768 minimum: 301 [ 0.000881] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000891] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes) [ 0.001422] Initializing cgroup subsys io [ 0.001438] Initializing cgroup subsys memory [ 0.001462] Initializing cgroup subsys devices [ 0.001474] Initializing cgroup subsys freezer [ 0.001485] Initializing cgroup subsys perf_event [ 0.001496] Initializing cgroup subsys pids [ 0.001521] CPU: Testing write buffer coherency: ok [ 0.001718] /cpus/cpu@0 missing clock-frequency property [ 0.001734] /cpus/cpu@1 missing clock-frequency property [ 0.001745] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000 [ 0.001780] Setting up static identity map for 0x800082c0 - 0x80008318 [ 0.080076] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001 [ 0.080138] Brought up 2 CPUs [ 0.080151] SMP: Total of 2 processors activated (24.59 BogoMIPS). [ 0.080157] CPU: All CPU(s) started in HYP mode. [ 0.080163] CPU: Virtualization extensions available. [ 0.080537] devtmpfs: initialized [ 0.107099] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0 [ 0.108008] omap_hwmod: l3_main_2 using broken dt data from ocp [ 0.305855] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.309769] pinctrl core: initialized pinctrl subsystem [ 0.310642] NET: Registered protocol family 16 [ 0.311543] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.340238] cpuidle: using governor ladder [ 0.370257] cpuidle: using governor menu [ 0.378384] OMAP GPIO hardware version 0.1 [ 0.384890] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 ! [ 0.408379] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers. [ 0.408390] hw-breakpoint: maximum watchpoint size is 8 bytes. [ 0.408836] omap4_sram_init:Unable to allocate sram needed to handle errata I688 [ 0.408846] omap4_sram_init:Unable to get sram pool needed to handle errata I688 [ 0.409405] OMAP DMA hardware revision 0.0 [ 0.451278] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported) [ 0.452379] edma 43300000.edma: memcpy is disabled [ 0.457084] edma 43300000.edma: TI EDMA DMA engine driver [ 0.460829] omap-iommu 40d01000.mmu: 40d01000.mmu registered [ 0.461009] omap-iommu 40d02000.mmu: 40d02000.mmu registered [ 0.461167] omap-iommu 58882000.mmu: 58882000.mmu registered [ 0.461324] omap-iommu 55082000.mmu: 55082000.mmu registered [ 0.461586] omap-iommu 41501000.mmu: 41501000.mmu registered [ 0.461762] omap-iommu 41502000.mmu: 41502000.mmu registered [ 0.464619] palmas 0-0058: Irq flag is 0x00000008 [ 0.481989] palmas 0-0058: Muxing GPIO 2f, PWM 0, LED 0 [ 0.564053] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz [ 0.564550] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz [ 0.564742] media: Linux media interface: v0.10 [ 0.564796] Linux video capture interface: v2.00 [ 0.564838] pps_core: LinuxPPS API ver. 1 registered [ 0.564845] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.564875] PTP clock support registered [ 0.564928] EDAC MC: Ver: 3.0.0 [ 0.565659] omap-mailbox 4883c000.mailbox: omap mailbox rev 0x400 [ 0.565940] omap-mailbox 4883e000.mailbox: omap mailbox rev 0x400 [ 0.566227] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400 [ 0.566505] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400 [ 0.566834] Advanced Linux Sound Architecture Driver Initialized. [ 0.567635] clocksource: Switched to clocksource arch_sys_counter [ 0.578527] NET: Registered protocol family 2 [ 0.579024] TCP established hash table entries: 8192 (order: 3, 32768 bytes) [ 0.579087] TCP bind hash table entries: 8192 (order: 4, 65536 bytes) [ 0.579212] TCP: Hash tables configured (established 8192 bind 8192) [ 0.579259] UDP hash table entries: 512 (order: 2, 16384 bytes) [ 0.579290] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes) [ 0.579507] NET: Registered protocol family 1 [ 0.579771] RPC: Registered named UNIX socket transport module. [ 0.579779] RPC: Registered udp transport module. [ 0.579786] RPC: Registered tcp transport module. [ 0.579792] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.580723] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available [ 0.583075] futex hash table entries: 512 (order: 3, 32768 bytes) [ 0.590698] squashfs: version 4.0 (2009/01/31) Phillip Lougher [ 0.591329] NFS: Registering the id_resolver key type [ 0.591356] Key type id_resolver registered [ 0.591364] Key type id_legacy registered [ 0.591425] ntfs: driver 2.1.32 [Flags: R/O]. [ 0.593371] bounce: pool size: 64 pages [ 0.593521] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247) [ 0.593537] io scheduler noop registered [ 0.593550] io scheduler deadline registered [ 0.593586] io scheduler cfq registered (default) [ 0.598497] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128 [ 0.659475] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled [ 0.662788] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 299, base_baud = 3000000) is a 8250 [ 1.521170] console [ttyS2] enabled [ 1.525826] [drm] Initialized drm 1.1.0 20060810 [ 1.532383] OMAP DSS rev 6.1 [ 1.536149] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops) [ 1.544587] omapdss_dss 58000000.dss: bound 58040000.encoder (ops hdmi5_component_ops) [ 1.560454] loop: module loaded [ 1.566295] libphy: Fixed MDIO Bus: probed [ 1.617667] davinci_mdio 48485000.mdio: davinci mdio revision 1.6 [ 1.623793] davinci_mdio 48485000.mdio: no live phy, scanning all [ 1.632488] davinci_mdio: probe of 48485000.mdio failed with error -5 [ 1.639607] cpsw 48484000.ethernet: Detected MACID = e8:eb:11:6e:e5:30 [ 1.646269] cpsw 48484000.ethernet: cpts: overflow check period 800 [ 1.653237] cpsw 48484000.ethernet: cpsw: Detected MACID = e8:eb:11:6e:e5:31 [ 1.661701] mousedev: PS/2 mouse device common for all mice [ 1.667857] i2c /dev entries driver [ 1.673995] gpio-fan gpio_fan: GPIO fan initialized [ 1.679316] tmp102 0-0048: error reading config register [ 1.684663] tmp102: probe of 0-0048 failed with error -121 [ 1.692969] omap_hsmmc 4809c000.mmc: Got CD GPIO [ 1.748130] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode [ 1.754515] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode [ 1.777771] vdd_3v3: supplied by regen1 [ 1.818918] ledtrig-cpu: registered to indicate activity on CPUs [ 1.831536] omap_hwmod: mcasp3: _wait_target_ready failed: -16 [ 1.837406] Unhandled fault: asynchronous external abort (0x1211) at 0x00000000 [ 1.837412] ------------[ cut here ]------------ [ 1.837426] WARNING: CPU: 0 PID: 6 at /home/gtbldadm/processor-sdk-linux-krogoth-build/build-CORTEX_1/arago-tmp-external-linaro-toolchain/work-shared/am57xx-evm/kernel-source/drivers/bus/omap_l3_noc.c:147 l3_interrupt_handler+0x25c/0x368() [ 1.837431] 44000000.ocp:L3 Custom Error: MASTER MPU TARGET L4_PER2_P3 (Read): Data Access in User mode during Functional access [ 1.837436] Modules linked in: [ 1.837442] CPU: 0 PID: 6 Comm: kworker/u4:0 Not tainted 4.4.32-gadde2ca9f8 #1 [ 1.837445] Hardware name: Generic DRA74X (Flattened Device Tree) [ 1.837457] Workqueue: kmmcd mmc_rescan [ 1.837461] Backtrace: [ 1.837475] [<c00130e4>] (dump_backtrace) from [<c00132e0>] (show_stack+0x18/0x1c) [ 1.837486] r7:c02e0670 r6:20000193 r5:00000000 r4:c0960dcc [ 1.837496] [<c00132c8>] (show_stack) from [<c02b420c>] (dump_stack+0x8c/0xa0) [ 1.837507] [<c02b4180>] (dump_stack) from [<c00349c4>] (warn_slowpath_common+0x88/0xb8) [ 1.837517] r7:c02e0670 r6:00000093 r5:00000009 r4:ee8adb48 [ 1.837527] [<c003493c>] (warn_slowpath_common) from [<c0034a2c>] (warn_slowpath_fmt+0x38/0x40) [ 1.837537] r8:00000017 r7:c0842020 r6:00000002 r5:c08420e0 r4:c0842184 [ 1.837546] [<c00349f8>] (warn_slowpath_fmt) from [<c02e0670>] (l3_interrupt_handler+0x25c/0x368) [ 1.837552] r3:ee9f5780 r2:c0842184 [ 1.837555] r4:80080003 [ 1.837565] [<c02e0414>] (l3_interrupt_handler) from [<c0080008>] (handle_irq_event_percpu+0xb4/0x160) [ 1.837576] r10:c098d572 r9:ee9ef840 r8:00000017 r7:00000000 r6:00000000 r5:ee9ef8a0 [ 1.837580] r4:ee9f5c80 [ 1.837589] [<c007ff54>] (handle_irq_event_percpu) from [<c00800f4>] (handle_irq_event+0x40/0x64) [ 1.837599] r10:00000000 r9:00000001 r8:ee808000 r7:00000000 r6:c093bdc4 r5:ee9ef8a0 [ 1.837603] r4:ee9ef840 [ 1.837612] [<c00800b4>] (handle_irq_event) from [<c0083420>] (handle_fasteoi_irq+0xc0/0x194) [ 1.837621] r7:00000000 r6:c093bdc4 r5:ee9ef8a0 r4:ee9ef840 [ 1.837629] [<c0083360>] (handle_fasteoi_irq) from [<c007f634>] (generic_handle_irq+0x2c/0x3c) [ 1.837637] r7:00000000 r6:00000000 r5:00000017 r4:c0931424 [ 1.837645] [<c007f608>] (generic_handle_irq) from [<c007f90c>] (__handle_domain_irq+0x64/0xbc) [ 1.837652] [<c007f8a8>] (__handle_domain_irq) from [<c000948c>] (gic_handle_irq+0x40/0x7c) [ 1.837663] r9:00000001 r8:fa213000 r7:fa212000 r6:ee8add08 r5:fa21200c r4:c09368e0 [ 1.837669] [<c000944c>] (gic_handle_irq) from [<c0013dc0>] (__irq_svc+0x40/0x74) [ 1.837673] Exception stack(0xee8add08 to 0xee8add50) [ 1.837679] dd00: 000004bf 00000000 df54e710 c0016e14 c09c3460 00001803 [ 1.837685] dd20: 02e59836 066665b0 ee8adde8 00000001 00000000 ee8add74 ee8add48 ee8add58 [ 1.837689] dd40: c02b1ff8 c0016e14 a0000013 ffffffff [ 1.837700] r9:00000001 r8:ee8adde8 r7:ee8add3c r6:ffffffff r5:a0000013 r4:c0016e14 [ 1.837706] [<c02b1fa4>] (__timer_delay) from [<c02b2030>] (__timer_const_udelay+0x28/0x2c) [ 1.837715] r7:066665b0 r6:c0960db4 r5:ee299000 r4:000001a9 [ 1.837724] [<c02b2008>] (__timer_const_udelay) from [<c04cf214>] (__mmc_start_request+0x88/0xdc) [ 1.837732] [<c04cf18c>] (__mmc_start_request) from [<c04cf360>] (mmc_start_request+0xf8/0x120) [ 1.837742] r9:00000001 r8:00000000 r7:ee8adea7 r6:ee299000 r5:ee299000 r4:ee8adde8 [ 1.837750] [<c04cf268>] (mmc_start_request) from [<c04cf420>] (__mmc_start_req+0x50/0x70) [ 1.837756] r5:ee8addf8 r4:ee8adde8 [ 1.837763] [<c04cf3d0>] (__mmc_start_req) from [<c04cf9d0>] (mmc_wait_for_cmd+0x60/0x8c) [ 1.837772] r7:ee8adea7 r6:00000000 r5:ee299000 r4:ee8ade34 [ 1.837781] [<c04cf970>] (mmc_wait_for_cmd) from [<c04da3c4>] (mmc_io_rw_direct_host+0x9c/0x138) [ 1.837788] r6:ee299000 r5:00000c00 r4:00000c00 [ 1.837795] [<c04da328>] (mmc_io_rw_direct_host) from [<c04da894>] (sdio_reset+0x2c/0x64) [ 1.837805] r10:ee8a8000 r9:00000000 r8:c06e3c2c r7:c06e3c20 r6:ee299000 r5:00061a80 [ 1.837809] r4:ee299000 [ 1.837816] [<c04da868>] (sdio_reset) from [<c04d1f98>] (mmc_rescan+0x274/0x318) [ 1.837820] r4:ee299258 [ 1.837830] [<c04d1d24>] (mmc_rescan) from [<c0049be4>] (process_one_work+0x124/0x3f4) [ 1.837841] r9:00000000 r8:eeb21400 r7:00000000 r6:ee8a8000 r5:ee85f000 r4:ee299258 [ 1.837850] [<c0049ac0>] (process_one_work) from [<c0049f00>] (worker_thread+0x4c/0x524) [ 1.837860] r10:ee8a8000 r9:ee85f000 r8:00000088 r7:ee8ac000 r6:ee8a8014 r5:ee85f018 [ 1.837864] r4:ee8a8000 [ 1.837872] [<c0049eb4>] (worker_thread) from [<c004fa58>] (kthread+0xe4/0xfc) [ 1.837883] r10:00000000 r9:00000000 r8:00000000 r7:c0049eb4 r6:ee85f000 r5:ee85e1c0 [ 1.837886] r4:00000000 [ 1.837894] [<c004f974>] (kthread) from [<c000fac8>] (ret_from_fork+0x14/0x2c) [ 1.837902] r7:00000000 r6:00000000 r5:c004f974 r4:ee85e1c0 [ 1.837916] ---[ end trace 4c7f855fa8bbe386 ]--- [ 2.280600] pgd = c0003000 [ 2.283315] [00000000] *pgd=80000080004003, *pmd=00000000 [ 2.288758] Internal error: : 1211 [#1] PREEMPT SMP ARM [ 2.294004] Modules linked in:[ 2.294761] mmc0: host does not support reading read-only switch, assuming write-enable [ 2.296697] mmc0: new high speed SDHC card at address 59b4 [ 2.307182] mmcblk0: mmc0:59b4 NCard 7.48 GiB [ 2.314881] [ 2.316560] CPU: 1 PID: 1 Comm: swapper/0 Tainted: G W 4.4.32-gadde2ca9f8 #1 [ 2.324769] Hardware name: Generic DRA74X (Flattened Device Tree) [ 2.330889] task: ee890000 ti: ee88c000 task.ti: ee88c000 [ 2.336314] PC is at __pm_runtime_idle+0x24/0x84 [ 2.340955] LR is at davinci_mcasp_probe+0x9bc/0xb60 [ 2.345941] pc : [<c03f4b44>] lr : [<c0548654>] psr: 20000013 [ 2.345941] sp : ee88dd10 ip : ee88dd30 fp : ee88dd2c [ 2.357466] r10: 00000000 r9 : 00000000 r8 : 00000000 [ 2.362712] r7 : ee8d1610 r6 : 00000000 r5 : 00000005 r4 : eea6ca10 [ 2.369266] r3 : eea6cad8 r2 : 00000000 r1 : 00000005 r0 : eea6ca10 [ 2.375822] Flags: nzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel [ 2.383161] Control: 30c5387d Table: 80003000 DAC: 55555555 [ 2.388930] Process swapper/0 (pid: 1, stack limit = 0xee88c210) [ 2.394961] Stack: (0xee88dd10 to 0xee88e000) [ 2.399338] dd00: ee2d0210 eea6ca10 00000000 ee8d1610 [ 2.407550] dd20: ee88ddc4 ee88dd30 c0548654 c03f4b2c 00002000 ee877710 ee2d0210 c0889cd8 [ 2.415763] dd40: 00000001 00000000 ee88dd6c 00000020 eed509a8 00000002 00000084 00000001 [ 2.423977] dd60: ee88dd8c ee8d0820 00000000 ee8d08c0 eea51c80 c0851c38 00000001 00000000 [ 2.432188] dd80: ee88ddb4 ee88dd90 c018413c c018095c eea6ca10 00000000 eea6ca18 c09cb81c [ 2.440400] dda0: eea6ca10 c098401c fffffdfb 00000000 c08e1600 00000000 ee88dde4 ee88ddc8 [ 2.448613] ddc0: c03ecfe8 c0547ca4 c09cb81c eea6ca10 00000000 c098401c ee88de0c ee88dde8 [ 2.456824] dde0: c03eb570 c03ecfa0 eea6ca10 c098401c eea6ca44 00000000 000000a8 c08e1600 [ 2.465037] de00: ee88de2c ee88de10 c03eb6f8 c03eb378 00000000 c098401c c03eb664 00000000 [ 2.473249] de20: ee88de54 ee88de30 c03e97f8 c03eb670 ee85bc5c eea4f734 ee85bc70 c098401c [ 2.481461] de40: ee8d1580 c0971710 ee88de64 ee88de58 c03eae5c c03e9794 ee88de8c ee88de68 [ 2.489672] de60: c03eaa98 c03eae44 c0891218 ee88de78 c098401c c0911508 c0939720 ee8774c0 [ 2.497885] de80: ee88dea4 ee88de90 c03ebe98 c03ea8fc c0971710 c0911508 ee88debc ee88dea8 [ 2.506096] dea0: c03ecf10 c03ebe24 c0939720 c0911508 ee88decc ee88dec0 c0911524 c03eced4 [ 2.514309] dec0: ee88df4c ee88ded0 c000978c c0911514 ee88def4 ee88dee0 c004ee88 c02bb160 [ 2.522520] dee0: effff600 c06a5ba4 ee88df4c ee88def8 c004f198 c08e160c ee88df34 c080cd50 [ 2.530733] df00: c080cd9c c080c5a8 00000006 00000006 00000000 c08dde74 c08717fc 00000000 [ 2.538944] df20: 00000474 c0990000 c0990000 c092f668 c0921834 000000a8 c08e1600 00000007 [ 2.547157] df40: ee88df94 ee88df50 c08e1f68 c0009700 00000006 00000006 00000000 c08e1600 [ 2.555367] df60: 00000000 c08dde74 00000000 c0990000 c066de94 00000000 00000000 00000000 [ 2.563580] df80: 00000000 00000000 ee88dfac ee88df98 c066deac c08e1da0 00000000 c066de94 [ 2.571794] dfa0: 00000000 ee88dfb0 c000fac8 c066dea0 00000000 00000000 00000000 00000000 [ 2.580006] dfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000 [ 2.588219] dfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000 [ 2.596427] Backtrace: [ 2.598894] [<c03f4b20>] (__pm_runtime_idle) from [<c0548654>] (davinci_mcasp_probe+0x9bc/0xb60) [ 2.607713] r7:ee8d1610 r6:00000000 r5:eea6ca10 r4:ee2d0210 [ 2.613442] [<c0547c98>] (davinci_mcasp_probe) from [<c03ecfe8>] (platform_drv_probe+0x54/0xb8) [ 2.622176] r10:00000000 r9:c08e1600 r8:00000000 r7:fffffdfb r6:c098401c r5:eea6ca10 [ 2.630079] r4:c09cb81c [ 2.632639] [<c03ecf94>] (platform_drv_probe) from [<c03eb570>] (driver_probe_device+0x204/0x2f8) [ 2.641545] r7:c098401c r6:00000000 r5:eea6ca10 r4:c09cb81c [ 2.647267] [<c03eb36c>] (driver_probe_device) from [<c03eb6f8>] (__driver_attach+0x94/0x98) [ 2.655738] r9:c08e1600 r8:000000a8 r7:00000000 r6:eea6ca44 r5:c098401c r4:eea6ca10 [ 2.663562] [<c03eb664>] (__driver_attach) from [<c03e97f8>] (bus_for_each_dev+0x70/0xa4) [ 2.671771] r7:00000000 r6:c03eb664 r5:c098401c r4:00000000 [ 2.677491] [<c03e9788>] (bus_for_each_dev) from [<c03eae5c>] (driver_attach+0x24/0x28) [ 2.685528] r6:c0971710 r5:ee8d1580 r4:c098401c [ 2.690195] [<c03eae38>] (driver_attach) from [<c03eaa98>] (bus_add_driver+0x1a8/0x220) [ 2.698238] [<c03ea8f0>] (bus_add_driver) from [<c03ebe98>] (driver_register+0x80/0x100) [ 2.706360] r7:ee8774c0 r6:c0939720 r5:c0911508 r4:c098401c [ 2.712079] [<c03ebe18>] (driver_register) from [<c03ecf10>] (__platform_driver_register+0x48/0x50) [ 2.721161] r5:c0911508 r4:c0971710 [ 2.724773] [<c03ecec8>] (__platform_driver_register) from [<c0911524>] (davinci_mcasp_driver_init+0x1c/0x20) [ 2.734726] r5:c0911508 r4:c0939720 [ 2.738336] [<c0911508>] (davinci_mcasp_driver_init) from [<c000978c>] (do_one_initcall+0x98/0x1e4) [ 2.747425] [<c00096f4>] (do_one_initcall) from [<c08e1f68>] (kernel_init_freeable+0x1d4/0x268) [ 2.756158] r10:00000007 r9:c08e1600 r8:000000a8 r7:c0921834 r6:c092f668 r5:c0990000 [ 2.764061] r4:c0990000 [ 2.766619] [<c08e1d94>] (kernel_init_freeable) from [<c066deac>] (kernel_init+0x18/0xf4) [ 2.774827] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c066de94 [ 2.782728] r4:c0990000 [ 2.785284] [<c066de94>] (kernel_init) from [<c000fac8>] (ret_from_fork+0x14/0x2c) [ 2.792883] r5:c066de94 r4:00000000 [ 2.796490] Code: e1a04000 0a00000a f57ff05b e28030c8 (f593f000) [ 2.802612] ---[ end trace 4c7f855fa8bbe387 ]--- [ 2.807359] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b [ 2.807359] [ 2.808382] mmcblk0: p1 p2 [ 2.819336] CPU0: stopping [ 2.822061] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G D W 4.4.32-gadde2ca9f8 #1 [ 2.830272] Hardware name: Generic DRA74X (Flattened Device Tree) [ 2.836392] Backtrace: [ 2.838864] [<c00130e4>] (dump_backtrace) from [<c00132e0>] (show_stack+0x18/0x1c) [ 2.846463] r7:c0935ef0 r6:20000193 r5:00000000 r4:c0960dcc [ 2.852185] [<c00132c8>] (show_stack) from [<c02b420c>] (dump_stack+0x8c/0xa0) [ 2.859443] [<c02b4180>] (dump_stack) from [<c0016420>] (handle_IPI+0x184/0x198) [ 2.866867] r7:c0935ef0 r6:00000000 r5:00000000 r4:c0931424 [ 2.872585] [<c001629c>] (handle_IPI) from [<c00094c4>] (gic_handle_irq+0x78/0x7c) [ 2.880185] r7:fa212000 r6:c0935ef0 r5:fa21200c r4:c09368e0 [ 2.885902] [<c000944c>] (gic_handle_irq) from [<c0013dc0>] (__irq_svc+0x40/0x74) [ 2.893416] Exception stack(0xc0935ef0 to 0xc0935f38) [ 2.898489] 5ee0: 00000001 00000000 00000000 c0020480 [ 2.906703] 5f00: c0934000 c09364ac 00000000 00000000 c0935f60 c0677224 c093650c c0935f4c [ 2.914914] 5f20: c0935f50 c0935f40 c0010554 c0010558 60000013 ffffffff [ 2.921553] r9:c0677224 r8:c0935f60 r7:c0935f24 r6:ffffffff r5:60000013 r4:c0010558 [ 2.929382] [<c0010518>] (arch_cpu_idle) from [<c00708b8>] (default_idle_call+0x28/0x34) [ 2.937511] [<c0070890>] (default_idle_call) from [<c0070b18>] (cpu_startup_entry+0x200/0x260) [ 2.946165] [<c0070918>] (cpu_startup_entry) from [<c066de90>] (rest_init+0x90/0x94) [ 2.953937] r7:00000000 [ 2.956492] [<c066de00>] (rest_init) from [<c08e1d88>] (start_kernel+0x400/0x40c) [ 2.964003] r5:c0990000 r4:c0990040 [ 2.967614] [<c08e1988>] (start_kernel) from [<80008090>] (0x80008090) [ 2.974166] r10:00000000 r9:412fc0f2 r8:80007000 r7:c093ab60 r6:c0921a24 r5:c0936484 [ 2.982069] r4:c0990214 [ 2.984624] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b [ 2.984624]