This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm365 mpeg4 codec issue

I found out that dynamic frame rate changes are not supported by the codec, but I am able to get it to work correctly by setting param->maxFrameRate to my desired frame rate and then manually dropping frames in the capture thread.  This allows the codec to correctly report bit rate.

 

I think I have also found another issue that arises when setting intraFrameInterval = 0.  The problem is that when encoding in this mode, I loose control over the bit rate.  Is there a workaround for this?  (Note: this is not an issue with H264 encoder codec).

 

Thank you!