Part Number: TCI6630K2L
Other Parts Discussed in Thread: RFSDK, , 66AK2L06
Hello,
So I am currently working on implementing the K2L chip in a system with a DAC over the JESD204B interface. I am currently working on using the DFE LLD included in the PDK to program and test the dfe basing my design off of the dfe and iqnet2 examples included with the PDK. These examples include a set of pre-configured DFE register values. I am assuming these are the same that the RFSDK stores in its tgtcfg files as the register addresses are mostly the same. I need to configure our DFE to accept 2 JESD RX pairs and 2 JESD TX pairs.
My problem is that the RFSDK includes configurations and target register configurations for only LTE and WCDMA applications. If I am doing our design for a custom signal size which target register configuration should I use for the DFE? Also where are the DFE configuration registers documented and if not why not?
Thanks so much!