Part Number: AM3358
Tool/software: Linux
Hi,
some issues in my custom board with dp83867, kernel cannot found phy device
in kernel log seems fine
[ 1.100566] libphy: Fixed MDIO Bus: probed
[ 1.164521] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6
[ 1.170670] libphy: 4a101000.mdio: probed
[ 1.175400] cpsw 4a100000.ethernet: Detected MACID = 98:5d:ad:7b:c3:5e
but in initial eth0 cannot found phy device
[ 6.349598] net eth0: initializing cpsw version 1.12 (0)
[ 6.356709] libphy: PHY 4a101000.mdio:00 not found
[ 6.361527] net eth0: phy 4a101000.mdio:00 not found on slave 0
[ 6.368144] libphy: PHY 4a101000.mdio:01 not found
[ 6.373016] net eth0: phy 4a101000.mdio:01 not found on slave 1
below is ifconfig response:
eth0 Link encap:Ethernet HWaddr 98:5D:AD:7B:C3:5E
inet addr:10.1.1.100 Bcast:0.0.0.0 Mask:255.255.255.0
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:174
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:0
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
here is my dts about network
&mac {
pinctrl-names = "default", "sleep";
pinctrl-0 = <&cpsw_default>;
pinctrl-1 = <&cpsw_sleep>;
status = "okay";
};
&davinci_mdio {
pinctrl-names = "default", "sleep";
compatible = "ti,cpsw-mdio", "ti,davinci_mdio";
pinctrl-0 = <&davinci_mdio_default>;
pinctrl-1 = <&davinci_mdio_sleep>;
status = "okay";
dp83867_0: ethernet-phy@0 {
reg = <0>;
ti,rx-internal-delay = <DP83867_RGMIIDCTL_2_25_NS>;
ti,tx-internal-delay = <DP83867_RGMIIDCTL_2_75_NS>;
ti,fifo-depth = <DP83867_PHYCR_FIFO_DEPTH_4_B_NIB>;
ti,min-output-impedance;
ti,dp83867-rxctrl-strap-quirk;
};
};
&cpsw_emac0 {
phy_id = <&davinci_mdio>, <0>;
phy-mode = "rgmii-txid";
};
&cpsw_emac1 {
phy_id = <&davinci_mdio>, <1>;
phy-mode = "rgmii-txid";
};