Part Number: PROCESSOR-SDK-AM437X
Hi there,
Is there an alternative to the old Starterware or CSL from the industrial SDK which can be used to test the hardware functionality of the AM437x HS EVM without having to use the entire linux-platform. I.e. make use of a simple signed bare-metal application which can run on the device to test functionality.
Best Regards
Eujean