Has the DMAI API been updated for h.264?
The reason I ask is becuase the "encoder" example in dvsdk_demos/dm365, which uses the DMAI API does not supply any h.264 specific parameters to the encoder. AND while there is a set of pre-defined parameters (Venc1_Params_DEFAULT) and dynamic parameters (Venc1_DynamicParams_DEFAULT), I can't find the equivalent defaults for the h.264 extended parameters or dynamic parameters.
Thx