This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: LCD configuration

Part Number: AM5728
Other Parts Discussed in Thread: TPD12S015, DS90CR217

Tool/software: Linux

Hello All,

Environment setup using:

OS: ubuntu 16.04

Ti-SDK:ti-processor-sdk-linux-am57xx-evm-04.02.00.09

I'm integrating 10.4"(800x600) display to our AM5728 custom board. Facing issue on lcd display bring up, please find the attached kernel log, config & dts file. 

Their is some problem with clarity, not sure issue with graphic driver side, weston side, RGB or resolution. Please go through attached file, snap shot once.

4540.AM5728.tar.gz

I commented the below lines in am57xx-beagle-x15.dts files: 

#if 0
&tpd12s015 {
gpios = <&gpio7 10 GPIO_ACTIVE_HIGH>, /* gpio7_10, CT CP HPD */
<&gpio6 28 GPIO_ACTIVE_HIGH>, /* gpio6_28, LS OE */
<&gpio7 12 GPIO_ACTIVE_HIGH>; /* gpio7_12/sp1_cs2, HPD */
};
#endif

If any changes required on dts, kernel config, please do let me know to bring up LCD.

Thanks.