Part Number: AM4376
Other Parts Discussed in Thread: SYSBIOS
Tool/software: Code Composer Studio
Hello,
I have done an application for the AM437x Starter Kit that was compiling well, without errors, using the following items and versions:
CCS 7.2
GCC ARM Compiler 4.9.3
processor_sdk_rtos_am437x 04.00.00.04
am437x PDK v1.0.7
bios 6.46.05.55
xdctools 3.32.02.25_core
Board: AM437x Starter Kit
Recently, I received a new computer and then I installed PDK again. The PDK installed on this new machine is the version 04.02.00.09. After importing the application done on the last version and compiling it, some errors related to gmake appeared. Below is a copy of the console showing the errors message:
xdctools_3_50_03_33_core\gmake.exe: *** [package/cfg/app_pa9fg.xdl] Error 1
js: "C:/ti/xdctools_3_50_03_33_core/packages/xdc/tools/Cmdr.xs", line 52: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[1]: *** [build-1811057185-inproc] Error 1
gmake: *** [build-1811057185] Error 2
gmake[1]: Leaving directory 'C:/ALSTOM/DSP/CED2/SRC/Teste_Board/Debug'
subdir_rules.mk:9: recipe for target 'build-1811057185' failed
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
After see these errors, I started to remove some parts of the application in attempt to discover where the problem was. I realized that the errors disappear when I remove some specific parts of the *.cfg archive. To be more accurate, the errors showed above disappear when I remove the lines of *.cfg related to NDK configurations and functions process that call xdc’s paths.
I’m using the items versions according to the PDK’s release notes. Below I’m listing the versions installed and that are in usage on the compilation of my application:
CCS 7.3.0.00019
GCC ARM Compiler v6.3.1
Processor_sdk_rtos_am437x 04.02.00.09
am437x PDK v1.0.9
bios 6.52.0.12
xdctools 3.50.3.33_core
Board: AM437x Starter Kit
Can someone help me to solve this?
Best regards.