Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/J6EVM5777: Problem with IPv6 over USB NCM interface

Part Number: J6EVM5777

Tool/software: Linux

Hi ,

Trying the follow up on the previous thread: e2e.ti.com/.../2318019

You concluded previously that IPv6 issue was with Android as Linux OS running on the same board did not have the problem.

Is there any updates on the issue?

Would updating to AO release (is using AM.1.3) help?

Also would the kernel patch and ConfigFS for CarPlay work the same on the AO release?

Thanks,

Alan